Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide22

Shown here is a screen shot of ADI’s amplifier parametric evaluation tool. In this example, the AD711 is used to model the effects of slew rate with a 4MHz input waveform. With a gain of 2, the output cannot keep up and the waveform is distorted. This tool is available on ADI’s website and is almost as accurate as a SPICE model. Notice that an error is flagged in orange to warn that this op amp is not suitable for this application. The tool is also capable of selecting an amplifier with the required performance characteristics for an application.

PTM פורסם ב: