Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide29

This is a graph illustrating the phase margin from a datasheet. Phase margin is the distance between the phase angle and the 180 degree mark at unity gain (or 0dB). If the phase margin decreases below 30 degrees, it is likely that the op amp will have a lot of overshoot. Many op amps datasheets will also plot phase margin over a range of temperatures.

PTM פורסם ב: