Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide23

One reason for using a feedback amp is to develop a closed loop gain that is independent of op amp characteristics. When bandwidth and slew rate are looked at, loop gain should also be considered. Gain error will be a problem at higher frequencies. Errors in the closed loop gain depend on the ratio between the open loop gain and the closed loop gain. So, as the signal frequency increases, the amount of gain will decrease as the closed loop gain gets closer to the open loop gain which results in increased gain error. This error causes distortion because it affects higher frequency signals more than lower frequency signals.

PTM פורסם ב: