Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide24

Shown here again is the AD711 amplifier with the same gain of 2, but with the frequency reduced to 2MHz. Looking at the gain bandwidth product and the slew rate, this amplifier can confidently create the output signal needed. However, a yellow error flag is thrown here as the gain error exceeds 1% because the closed loop gain is operating so close to the open loop gain at this frequency.

PTM פורסם ב: