Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide12

In an ideal op amp, there would be no current flowing into or out of the input pins. However, in a real op amp there are two sources of current. Bias current is the current that flows into or out of the input pins. Offset current is the difference between the current that flows to the inputs. When bias currents are very well matched, the offset current will be minimal. Bias current is normally much larger than the input offset current. Bias current is a problem for op amps because it can add errors when it flows through external resistance. For example, if the source impedance is 1MΏ, and the bias current of the op amp is 10nA, it will create a 10mV error. Or, if a signal is capacitively coupled to the op amp the bias current will charge the capacitor and stop working.

PTM פורסם ב: