Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide15

Auto-zero amplifiers and gain programmable amplifiers usually have the lowest possible drift. However, temperature drift can also be introduced through the feedback resistors. If one of the resistors is closer to a hot component, its resistance will change at a different rate then the cooler resistor resulting in a temperature drift error. If the resistors are integrated within the IC package, they will change at the same rate and the problem will be eliminated.

PTM פורסם ב: