Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide30

Another area of concern is 1/f noise. At higher frequencies, noise may be thought of as being evenly distributed, or white. But at very low frequencies the noise density increases. Most op amps will have a plot similar to this in their datasheet to show how the noise density rises as the frequency falls. Many op amps will specify the voltage or current noise from 0.1Hz to 10Hz or the corner frequency. The intersection of the dashed lines is the corner frequency of the op amp’s noise. When working with low frequency signals the effect of the 1/f noise over a limited area of the curve can be calculated by multiplying 6.6 by the RMS value.

PTM פורסם ב: