Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide9

Offset voltage is the first DC error this module will look at. Offset voltage adds a small voltage in series with the input signal. The offset voltage may be as small as a few microvolts, but it is multiplied by the op amp’s gain. Op Amp applications that require a high gain are more susceptible to offset voltage error than applications with low gain requirements. The offset voltage can be positive or negative, and is caused by a mismatching between the input transistors of the amplifier. To measure the offset voltage, the op amp is configured for a very high gain and the inputs are tied to ground. Then output voltage is then measured and divide by the noise gain.

PTM פורסם ב: