Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide21

Slew rate is the maximum rate of change of an amplifier’s output in response to a step change at the input. Shown here is a step change on the input, with the output of the op amp ramping up in response. Slew rate limits the bandwidth of large signals. It is a good idea to check the bandwidth of the part first, then check the maximum frequency the slew rate can support. The equation at the bottom of the slide can be used to calculate the maximum input frequency when the amplifier’s slew rate and peak output voltage are known.

PTM פורסם ב: