Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide32

Total noise is the combination of all uncorrelated noise sources and can be calculated by the root sum square method. Each term is squared, added, and the square root of the total is taken. If one noise source is three times larger than another, the smaller noise sources can be disregarded. To reduce the effect of the amplifier noise on other components in the system, the output of the amplifier can be filtered. The amplifier noise may occupy a very wide bandwidth, but a band pass, low pass, or high pass filter may be used to remove the unwanted noise.

PTM פורסם ב: