Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide28

Using a tank of water as an example, as the pump draws water from the bottom of the tank, the level will fall below the lower sensor. At this time, the valve will receive a command to open and refill the tank. But if the valve opens too slowly, the tank will run dry. When the tank is being filled, the upper level sensor will sense that it is time to turn off the valve. But if the valve closes too slowly, the tank will overflow. This is an example of phase margin, which is a way to measure response time. If the response time is too slow, the system can not keep up with the changes in the level. In this case, it takes so long to turn the valve on or off that the tank runs dry or overflows. For an op amp, if it takes too long for the output to respond to a change on the input, the outputs will oscillate.

PTM פורסם ב: