Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide7

Voltage feedback op amps are used in a wide variety of applications and are available in more varieties than current feedback. The perfect op amp would have an infinitely high input impedance which would ensure the op amp did not load the source (Vin), as well as having zero output impedance so it could drive any kind of load. It would also have infinite bandwidth and infinite open loop gain. Open loop gain is the total op amp gain with no feedback. Lastly, it would have no DC errors of any kind. Of course, there is no such thing as an ideal op amp.

PTM פורסם ב: