Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide49

In summary, op amps can be used in a wide variety of applications, but their most common application is simply to increase the amplitude of an AC or DC signal. There are two types of amps available: voltage feedback and current feedback. Voltage feedback is the most common, and responds to an error voltage between the inputs, while a current feedback op amp responds to a current error on the input. There are also many specifications to take into consideration when selecting an op amp and can vary greatly whether the part is used for high or low frequency applications.

PTM פורסם ב: