Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide17

The benefits of shielded vs. non-shielded inductors should be considered when making a selection. Shielded inductors offer low magnetic radiation for applications where low interference is deemed to be critical. The fewer number of winding turns, the lower the DC resistance. In contrast, non-shielded construction may be noisy. However, its inductance roll-off at DC current is much slower than a shielded inductor in a similar physical size. A higher number of turns are needed on non-shielded inductors which produces higher DC resistance than shielded inductors for the same amount of inductance.

PTM פורסם ב: