Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
QMEMS

Epson utilizes a photolithographic process called QMEMS to create uniformly shaped miniature crystal chips which are used in sub-miniature crystal units and crystal oscillators. As an example, for the same size 2.0 mm x 1.6 mm crystal unit, the QMEMS process provides outstanding temperature characteristics with minimal frequency variation compared to the conventional mechanical processing technique. As a reference, the QMEMS symbol is indicated next to products utilizing this technology in this presentation.

PTM פורסם ב: