Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Pt2-Slide11

If you are using a dsPIC33 device with 2 AD modules, you then have a lot of flexibility concerning how you allocate your AD module resources. If you select both AD modules as 10-bit, you will have 8 total sample and hold channels, capable of taking 8 simultaneous samples. The total conversion throughput of this system would be 2.2 mega samples per second. Another option is to configure both AD modules as 12-bit converters. Here, you will have 2 sample and hold channels, capable of taking 2 simultaneous samples and having a total conversion throughput of 1 mega samples per second. Another option is the configure one module as 10-bit and one module as 12-bit. This can provide flexibility of having high speed lower resolution conversions at the same time as lower speed higher resolution conversions.

PTM פורסם ב: