Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Pt2-Slide14

Let’s look at an example of setting up the PLL. Let’s assume that the source is a 4MHz crystal. We would like to run our device at 30MIPS. So, how to set up the PLL. First, we need to select a pre-scalar value. Since our source clock is relatively low frequency, let’s use the minimal divisor of two. This results in 2MHz into the phase comparator, which is within the 0.8 to 8MHz specified range, so this is OK.

PTM פורסם ב: