Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Pt2-Slide15

Since we want to run our system at 30MIPS, we want 30MHz out of our PLL. Since the VCO must output a frequency between 100 and 200MHz, we have to find a frequency that the VCO can run at which is a multiple of our 30MHz. The post-divisor can be either 4, 8 or 16 and if we choose 4, this will allow the VCO to run at 120MHz. This is within our range and 120 divided by 4 is 30MHz.

PTM פורסם ב: