Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Pt2-Slide13

Here’s a block diagram of the PLL module. The source frequency, originating from either the crystal oscillator, the precision internal RC or an external clock is input to the pre-scaling divisor.  This pre-scalar can divide by 2 through 32, selectable by a parameter in a special function register. To allow the module to function properly, the output of the pre-scalar must be between 0.8 to 8MHz. This frequency then goes to a phase comparator driving a VCO. The output of the VCO is routed through a divisor that also drives the phase comparator. The value of this divisor corresponds to the multiplication factor of the PLL. The divisor can divide by 2 through 514, again selected by a parameter in a special function register. Note that the output of the VCO must be within 100 to 200MHz. The output of the VCO is routed to a post-scalar divider, which can divide by either 4, 8 or 16.

PTM פורסם ב: