Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Pt2-Slide22

Generally, if none of the new features of the peripheral modules is used, then there is no requirement to update any of the software associated with the peripherals. However, significant gains in system performance can be achieved by using the DMA system. Interfacing to CAN bus systems is easier utilizing the new features of the enhanced CAN. And the new features in other communication modules can enable simpler utilization of LIN bus, IRDA, SPI and I²C protocols in the system. The dual mode AD module along with the increased number of analog inputs simplifies signal conversion.

PTM פורסם ב: