Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Flash and SRAM

Flash is one of the key differentiating elements of the NXP microcontrollers and is an important factor in the huge success of the family. The NXP Flash is the highest performing flash available on an ARM7 microcontroller, performing 37% to 51% faster than its competitors. This is because NXP’s Flash has the ability to execute code at frequencies up to 72 MHz with zero wait states.

PTM פורסם ב: