Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
ARM
NXP currently has the largest ARM microcontroller family in the market today with the LPC2000 family. The LPC2300 and LPC2400 series of microcontrollers are based on the ARM7TDMI-S core. The suffix TDMI-S describes some of the features on this new ARM7 core. This core includes a Thumb architecture and debug extensions, an enhanced multiplier (32 x 8) that can yield 64-bit results, EmbeddedICE Macrocell to support in-circuit emulation, and fully synthesizable soft IP so standard off-the-shelf MCUs can be used rather than a design with a hard IP core.
PTM פורסם ב: