Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
MAM 2

This simplified illustration of the MAM shows that it is made up of three 128-bit buffers. The Prefetch buffer eliminates any code fetch penalty for sequential instructions by loading four 32-bit (or eight 16-bit) words via the 128-bit wide interface to Flash. This is initiated as soon as Flash completes the previous access. The Branch Trail buffer captures the line when a code branch occurs. When the branch occurs again, those instructions are already available in the branch trail buffer. The Data Bypass buffer serves subsequent data requests which are satisfied from the Data Bypass latch if the data is sequential between the previously and next fetched data.

PTM פורסם ב: