Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Power Modes 2
In addition to the various methods of reducing power in active mode, the ARM7 core supports various power reduction modes including Idle, Sleep, and Power Down. In Idle mode, the core is stopped but the peripherals remain in operation. In Sleep mode, the MCU receives no internal clocks whatsoever but the processor state is retained with the registers, logic levels, and RAM content.The Flash and RTC remain as well, unless disabled. With the internal RC (IRC) oscillator, the MCU can come out of Sleep mode in only four clock cycles. Finally, Power Down mode is very similar to Sleep mode except that the Flash and RTC are both turned off. With an IRC, the MCU can wake up in 60 μs + 4 clock cycles.
PTM פורסם ב: