Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
MAM

The Flash achieves this success margin through the NXP proprietary Memory Accelerator Module (MAM). The normal Flash access time is approximately 50 ns, so execution out of Flash even with zero wait is 20 MHz maximum.  In order to execute at 72 MHz, NXP developed and implemented the MAM instead of a cache due to the deterministic nature of the MAM.  With a cache, a user cannot always predict how long an instruction will take to execute, whereas MAM is deterministic and repeatable. The MAM also has an enable/disable feature and different programmable modes.

PTM פורסם ב: