Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Indepen Bus

The LPC2300 and LPC2400 have three independent high speed buses: the local bus, Amba High Speed Bus 1 and Amba High Speed Bus 2. The local bus connects the ARM core with the zero wait-state Flash and is the highest speed bus in the ARM7 architecture. The Amba bus 1 supports the USB and LCD controllers while handling USB packet reception and LCD frame transfer from internal or external SRAM to the LCD panel. The Amba bus 2 is dedicated to Ethernet packet reception and transfer to the SRAM. By operating independently, these busses can handle the large amount of data transfer that can occur when the peripherals operate concurrently. 

PTM פורסם ב: