Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Power Modes
The ARM7 core requires 1.8 V to operate and the I/O and peripherals requires 3.3 V. The LPC2300 and 2400 series has an on-chip DC-DC converter so only the 3.3 V supply is required as the core power will be supplied by the on-chip DC-DC converter. If the RTC is operated in power down mode, then power needs to be supplied to the RTC as well. To minimize power consumption, the core can be configured with modified clock sources, reconfigured PL values, altered CPU clock divider values, and divided or shut off clocks to individual in-chip peripherals. 
PTM פורסם ב: