Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Embed Flash

In addition to the MAM, there are a number of other features that make the LPC2000 Flash unique. The LPC2300 and LPC2400 MCUs use a proprietary 0.14 micron, eFlash technology which provides low cost and low power. The Flash is comprised of two transistor NOR cells which provide high reliability, qualifying the Flash for many harsh environment automotive products throughout NXP. Additionally, the Flash has 8-bits of error correction for every 128 bits of Flash. This provides for single-bit error correction in the Flash. The code can also be secured through different levels of code read protection.

PTM פורסם ב: