Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide37

To reinforce the geometry requirements of the PCB, the radiation of the board and the radiation of the element make the sum of the total radiation from the device. As the aperture of this board is reduced, especially with respect to the wavelength of the antenna, the antenna aperture made up of the PCB is reduced.  This causes all other performance figures to decrease as well.

PTM פורסם ב: