Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide9

When applying the ceramic PIFA, the ideal location is centered on the length of the PCB. The second best location would be within no less than 10mm of the top or bottom edge along the width of the board. The E-Plane is in the same vertical plane as the length of the PCB, therefore the radiation pattern is best suited for applications in which the device orientation may be other than vertical. The typical radiation efficiency of the ceramic PIFA is greater than 70%.

PTM פורסם ב: