Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide43

The ground pour consistency on the PC board is important because the entire PC board is the ground plane for the antenna, and the overall PCB dimensions determine the electrical length. The ground pour around the ground clearance (GC) area needs to be particularly solid. Through the use of vias, the ground pour does not need to be continued in the same layer throughout the PC board. 

PTM פורסם ב: