Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide46

Part of proper grounding on the PCB includes the metallic components such as a display, shield cans and mechanical supporting structures which may cause loss of radiation if not properly grounded. Antenna signal can couple to these components, particularly if there is gap between the PCB and the metallic component. These gaps can create a high-loss, non-radiating resonance in or out of the band which lowers the antenna efficiency. Close-to-band resonances are especially harmful. It may even appear that antenna matching is improved due to these resonances, but in the worst case, they can reduce the radiation significantly.

PTM פורסם ב: