Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List Associated Content
Industrial Motor Drive Applications

Examples of industrial motors are shown in the chart and images on this slide. Industrial motors can be categorized based on their input power supplies. Those powered from AC voltages can be further classified depending on the voltage level and gate drive isolation topology. These AC motors are mainly found in factories and commercial buildings. Some motors also operate from DC voltages using onboard batteries, such as those for e-mobility applications.

PTM פורסם ב: