Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
L99ASC03 Fully-Integrated Motor Driver IC for Three-Phase Brushless Motors Slide 21

Built in Back-EMF detection is optimized for six-step drive mode. There is no need for additional external sensors or components for this function. Pre-commutation allows for very fine control of the motor in a dynamic control scenario where the commutation has to be setup before it actually happens. This can be done up to 45 degrees. Back-EMF detection can be done both during PWM on and off from 0% all the way up to 100% duty cycle. Additionally, the motor does not have to be powered for the function to operate, and a feature in the algorithm allows the device to determine the position of the rotor at any given time. The microcontroller resources required for Back-EMF detection are limited to one general purpose IO pin, a significant advantage.

PTM פורסם ב: