Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
L99ASC03 Fully-Integrated Motor Driver IC for Three-Phase Brushless Motors Slide 7

There are two methods to detect Back-EMF. Starting with the conventional method first, which is based on neutral point voltage. When two phases are conducting current, the third winding is floating. So the back-EMF of the floating winding can be detected. Usually, the back-EMF voltage is referred to the motor neutral point. For this method, the terminal voltage is compared to the neutral point, and the zero crossing of the back-EMF can be obtained. In most cases however, the motor neutral point is not available, so a virtual neutral point is built by resistors. It looks pretty nice; however, it has a few problems.

PTM פורסם ב: