Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
TPS75005 Integrated Solution for C2000 MCUs Slide 19

The next step is to connect the third internal supervisor, SVS3. The first two supervisors control rails one and two, the third can be used to monitor the input voltage for any glitches coming in from the source. When SVS3 is not being used it is connected as shown in the diagram on this slide.

PTM פורסם ב: