Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
TPS75005 Integrated Solution for C2000 MCUs Slide 8

The drawback of a linear solution over a switcher based solution is the efficiency. If the customer’s key concern is not efficiency, the TPS75005 would be a better solution. Shown on this slide and the next, is the data that supports 40% BOM saving between the two solutions as a reference. This slide shows the space requirements of a switcher based solutions.

PTM פורסם ב: