Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide13

Electricity passing through any material encounters an opposing force that is similar to mechanical friction. This opposing force in a conductor is called resistance. The value of the resistance is determined by the conductor size and material. In direct current (DC) applications resistance limits the length of the cable because of the voltage reduction caused by resistance. In digital applications, resistance contributes to the characteristic impedance and is the primary cause of voltage loss (attenuation). Cable resistance is specified in Ohms per foot (Ω/ft).

PTM פורסם ב: