Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide21

In a balanced system the data contained in a series of pulses is input to the driver. The driver reproduces these pulses both in positive and negative form, and sends the positive data pulses down one conductor and the corresponding negative data pulses down the other conductor. If noise is picked up by the conductors, it is picked up equally by both. The receiver inverts the pulses from one of the conductors and algebraically adds them with the pulses from the other channel. The pulses are now at the same polarity and add up. The noise spikes, on the other hand, are now of opposite polarity and subtract, resulting in the noise being cancelled out with no error occurring. This noise cancellation is referred to as common mode rejection.

PTM פורסם ב: