Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide26

Twisted pair transmission line was created by twisting two discrete wires together. The twisting provides good immunity from magnetic fields created by motors, relays, transformers and so on. Twisted pair exhibits good cross talk reduction, especially when driven balanced. Twisted pair cables are available as parallel lay where the conductor pairs are laid side by side in their respective insulations along the entire length of cable. These are also offered in flat or round jackets, with or without shields.

PTM פורסם ב: