Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide17

Impedance matching can perhaps be explained by comparing the pulse traveling down the cable to water flowing through a pipe. Imagine a section of pipe, one inch in diameter, welded to a section of pipe, one half inch smaller in diameter. If water were to flow through these welded pipes the change in diameter would cause a disturbance in the flow. In the same manner, a cable with mismatched impedance would create a disturbance in the ‘flow’ of the signal. The disadvantages of not having a matched system are: the pulse does not reach the output; and increased noise.

PTM פורסם ב: