Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide34

Shield conductivity and proper termination of that shield are the two critical factors in protection from ESD. Shielded jacketed cables from 3M use low resistance copper shields for maximum protection. This chart shows the variations observed while evaluating different termination techniques. Clearly the best shielding is achieved when clamping the shield directly to the metal cabinet, but this is not a practical solution in an I/O application where the cable may need to be disconnected during installation or maintenance. Using a drain wire ground induces a voltage 26 times that of the clamped shield. A compromise between shielding conductivity and usability is a terminated connector in an assembly such as a back shell with jack screws.

PTM פורסם ב: