Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide22

Now turning to external interference, electricity travels through space as electro-magnetic energy. When a licensed broadcaster, such as a radio station, is transmitting and a user’s radio is able to pick up good reception, it is considered desirable energy. If their neighbor is operating a high-powered drill which emits electro-magnetic energy in his garage, and it interferes with radio reception, it is considered undesirable energy or electro-magnetic interference (EMI). Manufacturers of computers have always had to deal with received electro-magnetic energy by using shielding, noise immune logic or balanced drives. Due to the proliferation of digital logic, home computers, printers, electronic games, MP3 players, mobile cell phones and so on, the Federal Communications Commission (FCC) of the United States regulates electro-magnetic emissions of these digital devices so that they do not interfere with licensed broadcasts, wireless phone service, medical equipment in hospitals and radio communications frequencies used by emergency services. In other countries statutory authorities enforce similar regulations.

PTM פורסם ב: