Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
SAM3U-PowerMgmt-Slide10

The general purpose DMA embeds four channels, three channels with 8 bytes of FIFO for channel buffering and one channel with 32 bytes of FIFO. It supports a wide range of transfer types, including memory-to-memory or peripheral-to-memory transfers for the SPI, SSC and MCI. A new feature of DMA implementation on the SAM3U is that the it can be triggered by the PWM controller or any Timer Counter channel to generate a waveform through the External Bus Interface.

PTM פורסם ב: