Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
SAM3U-PowerMgmt-Slide7

The PWM controller on the SAM3U integrates new features that are particularly useful for motor control applications, such as PDC support, complementary outputs, fault inputs providing asynchronous protection of PWM outputs and dead-time generators. It is also possible to drive the power management controller when the crystal oscillator fails, thus providing protection for the different PWM outputs. 

PTM פורסם ב: