Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Xplained-Slide11
Microchip's sensors software incorporates all the necessary drivers for all supported sensors. This enables a standardized programming interface for development on all the Microchip Xplained hardware boards. Furthermore, the calibration routines of the sensors are included and ready to be used by the customer application. The data returned from the sensors software is not just a number, but a number with a unit like for example mg (milli-g) for acceleration or °/S for rotation. This makes it easier to develop software as the developer does not need to figure out the scaling factor of the output from the different sensors. In short, the sensor drivers provide an interface for all the sensors with configuration and setup, and output normalized into engineering units.
PTM פורסם ב: