Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Xplained-Slide5

The UC3-L0 Xplained development board is a typical Xplained board with two board controllers. The target microcontroller on the board is the UC3L064. All deployed sensor applications will run on the main microcontroller. The second board controller is used to control the USB port as this is very useful for the development process. In addition to the USB port there is a programming port for JTAGICE programming tools, a header to directly measure current consumption and four ports for use with the sensor top boards. J1 and J4 are digital ports, J2 is an analog port with eight channels and J3 is a general purpose I/O port. These four ports are common to all of the boards making all sensor top boards compatible with all of the microcontroller boards.

PTM פורסם ב: