Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
atmel-xplained

The sensor boards on this slide aim at the growing market for inertial sensors. Inertial navigation systems use accelerometers, magnetometers and gyros to calculate the position, orientation and velocity of a moving object without the need for external references. The inertial sensor boards one and two have the same type of sensors, but the sensors are made by different manufacturers and thus have different capabilities. It is not necessary to make changes to the program code to switch between the two top boards. Simply exchange the top board and recompile the application for the new sensor board.

PTM פורסם ב: