Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Xplained-Slide12

The output from the sensors is automatically scaled. The chosen units are the common SI units. This function can be turned off and the application will receive raw data instead. The sensors output two types of data: vector based sensor data, for example the accelerometer and the gyroscope output direction data as well as magnitude; and scalar sensor data, for example temperature and pressure is presented as one single scalar value. In addition, the software drivers provide a timestamp, in µS, associated with every data reading. The latency of the reading is also available as this is important for some applications. 

PTM פורסם ב: