Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Xplained-Slide22
The data visualizer tool will give a more user-friendly presentation of the data from the senor board. This interface consists of real-time updated graphs representing the different output parameters of the sensors. The visualizer will use all of the function calls available in the API. In Atmel Studio 6 choose a new example project, then technology and Mems sensor. A list of example pojects will now be disploayed. Choose the Sensor Data Visualizer project, re-connect the JTAG cable, build and download the project. Once the files are downloaded, unply the JTAG cable. Finally start the PC program called Microchip Data Visualizer. This program is associated with Atmel Studio 6, but is the separate download available at Microchip.com. An application note on how to use the visualizer can be downloaded together with the program files. Make sure the mini-USB cable is connected and select the appropriate Com port.
PTM פורסם ב: